4/16/2019 1:45 PM | |
Posts: 25 Rating: (0) |
is it possible to insert a drop down or a wild card to a function block in tia portal provided PLC is siemens 1214 and software is TIA V15 as for example, in a "convert" instruction there will be an automatic drop down to select the data type of source and destination.(please refer the attachment) in such a way, is it possible to add drop down list to a user made function block ------------------------------------------------------------------------------------------ |
Last edited by: Rakeysh at: 4/16/2019 1:46:50 PMLast edited by: Jen_Moderator at: 4/16/2019 2:12:21 PMNew subject after splitting Last edited by: Rakeysh at: 4/17/2019 7:02:20 AM |
|
4/18/2019 6:07 PM | |
Joined: 7/7/2010 Last visit: 9/20/2024 Posts: 15213 Rating: (2417)
|
The closest thing that comes to mind is the use of "Variant" as a datatype. Inside the block, the plc checks the datatype of the provided parameter. If it matches a given datatype, it can then execute datatype specific logic, or set some flag to indicate the datatype for use elsewhere within the block. F1-Help on various "isxxxx" instructions, and how they can be used.
|
science guy |
|
4/22/2019 3:31 PM | |
Joined: 7/7/2010 Last visit: 9/20/2024 Posts: 15213 Rating: (2417)
|
See attached zip. For some reason, I could not reliably post the png image inside the zip. It posted once, but when I hit preview, I lost it.
AttachmentFavorites_Ladder.zip (133 Downloads) |
science guy |
|
4/24/2019 3:36 AM | |
Posts: 25 Rating: (0) |
I couldn't open the file |
Follow us on