9/7/2014 4:25 PM | |
Joined: 6/14/2013 Last visit: 3/18/2023 Posts: 218 Rating: (9) |
Hello, This program is for managing the skip of the concrete plant. Rising skip, lowering skip, skip waiting at halfway. Is it correct? Thank you for any advice AttachmentSkip.zip (205 Downloads) |
9/7/2014 7:31 PM | |
Posts: 5225 Rating: (1185) |
Hi there, The attached image has some comments to what the program is intended for. Hopefully these will provide good ideas. I hope you are not colour blind.. that may give problems. The upward motion can be stopped before reaching the top stop position. The position is indicated on the image (sea-green colour). Check back with us.. if you wish to do so. Greetings. w AttachmentVisual Clue_Design ideas for SKIP motion.zip (178 Downloads) |
This contribution was helpful to1 thankful Users |
9/8/2014 12:53 AM | |
Joined: 6/14/2013 Last visit: 3/18/2023 Posts: 218 Rating: (9) |
um ... I'm saturated, out!
Attachmentskip_2.zip (152 Downloads) |
9/9/2014 7:14 PM | |
Joined: 6/14/2013 Last visit: 3/18/2023 Posts: 218 Rating: (9) |
Third attempt to improve the program ...?
Attachmentskip3.zip (166 Downloads) |
9/9/2014 7:38 PM | |
Posts: 5225 Rating: (1185) |
Hi there, Please find my commentary attached. Especially in the documentation there is very good progress. It would seem as though the idea is there (in planning). Unfortunately the coding is not following the planning and contains errors. You still have a way to go.. but you are on the right track. What demotivates me in helping further is that you have not taken seriously my suggestion of working the steps out on a spreadsheet. (Libre Office is for free.. if that is the problem.) It does not matter what shorthand you use for indicating timers or such, but I strongly believe it could help you. I have writers-block sometimes.. having a non-programming method to assist helps a lot. It does not even have to be a spreadsheet - flow charts can also help for example. I hope other members contributes to help you.. they are welcome to do so. Probably I will not be available for a while as per my own work related priorities. Good luck. w AttachmentCOMMENTARY ON SKIP3.zip (197 Downloads) |
This contribution was helpful to1 thankful Users |
9/10/2014 7:46 AM | |
Posts: 5225 Rating: (1185) |
..sample for the back end of the movement control: "Design Idea_Movement control back end.PNG" AttachmentDesign Idea_Movement control back end.zip (158 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on