12/19/2015 6:30 AM | |
Posts: 111 Rating: (1) |
ladder logic to start/stop motor using only one momentary NO push button Can anybody do this for me? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 12/21/2015 1:59:10 PMNew subject after splitting |
|
12/21/2015 2:22 PM | |
Posts: 5225 Rating: (1185)
|
|
Last edited by: William_B at: 12/21/2015 2:43:38 PM |
|
This contribution was helpful to2 thankful Users |
12/21/2015 3:04 PM | |
Joined: 9/2/2008 Last visit: 2/21/2024 Posts: 191 Rating: (43) |
Or this simple one |
Problems don't exist, only challenges. |
|
This contribution was helpful to2 thankful Users |
12/21/2015 4:59 PM | |
Joined: 7/7/2010 Last visit: 4/26/2024 Posts: 14639 Rating: (2349)
|
Attached is an untested (for reliability) piece of code that allows for selecting whether the input state change is edge detection for toggle, or delayed (by 0.1 sec) for debounced state change. It compiles is the best I can say. It may be buggy in your application so use with caution. AttachmentForums_Toggle_NO_Input.pdf (990 Downloads) |
science guy |
|
This contribution was helpful to2 thankful Users |
Follow us on