2/20/2018 8:06 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1051) |
hi together, Win 10 is not supported by TIA V13 SP1 You need at least V13 SP2. SIMATIC STEP 7 including PLCSIM V13 SP2 TRIAL download The license-error are caused by Fall creators update for win10. Encryption can´t be terminated correctly. It can be done manually: Close all Siemens applications. Close Automation License Manager service in Windows control center. Open the folder "C:\ProgramData\Microsoft\Crypto" Change the name of the folder "DSS\MachineKeys“, "RSA\MachineKeys“ and "RSA\S-1-15-18“. like "DSS\MachineKeys_old“, "RSA\MachineKeys_old“ and "RSA\S-1-15-18_old“ Restart the system. Check if the Automation License Manager service is started again. Check If the Licenses are shown correct. If everything is alright you can delete the old folders. hope this helps, regards, |
FCK WAR! |
|
This contribution was helpful to5 thankful Users |
3/14/2018 1:13 PM | |
Joined: 10/12/2007 Last visit: 3/22/2024 Posts: 12 Rating: (0) |
This fix works also with TIA Portal V14 SP1 + Windows 10 build 1709. |
This contribution was helpful to1 thankful Users |
10/5/2018 1:06 PM | |
Joined: 10/5/2018 Last visit: 11/12/2022 Posts: 3 Rating: (0) |
This also works with TIA 15 and windows 10 |
Follow us on