4/8/2016 11:53 AM | |||||||||
Joined: 3/28/2015 Last visit: 4/19/2024 Posts: 721 Rating: (213) |
Hello, Kindly have a look at the following topic:
|
||||||||
Eng.Mohamed Ibrahim |
|||||||||
This contribution was helpful to1 thankful Users |
4/8/2016 12:22 PM | |
Joined: 5/28/2008 Last visit: 4/15/2024 Posts: 4505 Rating: (835) |
Dear friend, In this entry, Siemens announce 32MB MC for delivery for S71200 + ...... Delivery release for 32 GB SIMATIC Memory CardDate of above entry was: 24 Aug. 2015 And also in the following entry Siemens state memory cards released for S7-1200 which only 2MB , 4MB and 24MB Usage of S7-1200 Memory CardDate of above entry was: 26 March 2014 It sound logical that Siemens enlarged the MC capacity, but before ordering please check the comptability between MC and your CPU version. |
Last edited by: Ayman Elotaify at: 4/8/2016 12:22:33 PMAyman Elotaify |
|
This contribution was helpful to1 thankful Users |
4/8/2016 12:26 PM | |||
Joined: 5/12/2006 Last visit: 4/19/2024 Posts: 22213 Rating: (2979) |
not compatible with V3!
|
||
This contribution was helpful to1 thankful Users |
4/8/2016 12:31 PM | |
Joined: 5/12/2006 Last visit: 4/19/2024 Posts: 22213 Rating: (2979) |
only the access limitation in windows explorer was no longer valid the cards have a modified MBR and Partiton table which is destroyed with diskpart. a 2MB Card for S7-1200 have a capacity of 32 MB and 2 Partitons (3MB and 1 MB unused), so is similar to the old MMC of S7-300, same HW Type of card and the capacity is limited with MBR and Partitontable.
Christoph |
This contribution was helpful to2 thankful Users |
4/8/2016 12:34 PM | |
Posts: 8946 Rating: (999) |
Thanks a lot, that was very helpul! |
Follow us on