4/13/2016 12:56 PM | |
Posts: 22 Rating: (0) |
Hello, I need to make a motor holding brake with the MM420, Can it do it by itself or dou I need an external break? Thanks for the help. Regards |
4/13/2016 1:15 PM | |
Joined: 6/4/2008 Last visit: 4/23/2024 Posts: 1481 Rating: (322)
|
Perhaps the section in the MM420 Operating Instructions Labelled "Motor Holding Brake (MHB)" might have some clues |
4/14/2016 9:02 AM | |
Posts: 22 Rating: (0) |
Thanks for the answers, Yes, it's vertical axis. And i have an external brake, but i can't find how to command it. |
4/14/2016 11:09 AM | |
Posts: 6 Rating: (0) |
Hello, you need external brakes that need to be powered from the Drive output terminals points. BR ZH |
4/15/2016 8:01 PM | |
Posts: 22 Rating: (0) |
The coil burnt because of a wrong supply voltage. thanks for your concern |
This contribution was helpful to1 thankful Users |
Follow us on