7/4/2018 9:50 PM | |
Posts: 2826 Rating: (685) |
Hello.
I do not know the answer. What I do know is that there are variants of the drives when it comes to communication modules. The communication protocol might be a bigger issue than the actual software. - Which communication is available for your drive? web searching "communicate PC micromaster 440" delivers: BR |
7/5/2018 5:20 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello, You might have refered the link mentioned in reply by forum memebr #dP. However please refer the below link if you could not access the link. Uploading and downloading drive parameters of a MICROMASTER 4xx using STARTER (1,5 MB)
AttachmentUpload_download_MM4_parameter_using_STARTER_en.pd.pdf (239 Downloads) |
Last edited by: Jen_Moderator at: 7/5/2018 6:45:50 AMAdded file as an attachment. |
|
Follow us on