9/16/2011 12:14 AM | |
Posts: 6 Rating: (0) |
I can use MW255 but I can not use MW2000 while I have 128 KB memory. What can be the problem? |
9/16/2011 1:35 AM | |
Joined: 5/28/2008 Last visit: 4/15/2024 Posts: 4505 Rating: (835) |
Hello bates, It is depends on which CPU you have. For instance, if you haveCPU312, then the Max. Flags is 256 bytes (i.e. from MB0 to MB255). if you haveCPU315-2DP, then the Max. Flags is 2048 bytes (i.e. from MB0 to MB2047). Hope this helps. |
Ayman Elotaify |
|
9/16/2011 11:10 AM | |
Posts: 6 Rating: (0) |
I am using |
9/16/2011 11:22 AM | |
Joined: 4/24/2006 Last visit: 4/15/2024 Posts: 8610 Rating: (1146) |
Hello, The mentioned CPU, also has Flags 256 byte. See this link: http://support.automation.siemens.com/WW/view/en/42361392/td The mentioned CPU has 192 Kbyte workmemory. To use all of it, you should have a MMC of 512 Kbyte. (Load memory should be larger than Workmemory) Best regards, Wizard |
9/16/2011 1:38 PM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating: (270) |
Dear bates, |
Last edited by: Amit_86 at: 9/16/2011 1:43 PMLast edited by: Amit_86 at: 9/16/2011 1:40 PMVANDE MATARAM..... |
|
Follow us on