3/13/2020 10:49 AM | |
Posts: 6 Rating: (0) |
Hey guys, i want to establish a Modbus TCP connection between S7-1200 and Nanotec Motorcontroller with module MB_Client. For testing I use EasyModbusServer. There is no connection. Instead the output "busy" is always "true" and "done" is always "false". I hope someone has a solution for this problem! Thanks in advance! AttachmentDesktop.zip (110 Downloads) |
3/13/2020 12:10 PM | |
Posts: 6 Rating: (0) |
Thanks for the answer! Which connection settings do you mean? Is it the "ActiveEtablished" setting in the "MB_Config_Client" ? |
3/13/2020 1:06 PM | |
Posts: 6 Rating: (0) |
I changed the Ports as you mentioned. The RemotePort is 502 and the Port at the PC sim is 502 as you can see in the screenshots. But the "busy" output remains "true" and there is no connection. Was that the problem that you meant? Or do I have to change something different? Attachment3.zip (113 Downloads) |
3/15/2020 11:00 AM | |
Posts: 6 Rating: (0) |
Thank you very much for your help, duris_I ! I will try out your tipps. |
This contribution was helpful to1 thankful Users |
Follow us on