11/16/2012 7:07 AM | |
Joined: 9/6/2008 Last visit: 5/7/2022 Posts: 1121 Rating: (86) |
HI Well can you give a screen shot for the error. Have fun... |
Jazz |
|
11/16/2012 4:14 PM | |
Joined: 10/12/2010 Last visit: 3/10/2022 Posts: 4 Rating: (0) |
Error shown in attachment.If I delete the second rung in Network 1 all is fine... |
11/16/2012 4:57 PM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365)
|
Hello , There are rules for creating logics in LAD and it is compulsory to follow them.In STEP7,LAD editor will not allow you to create wrong logics in Nature in most of the time. For your case in TIA Portal,error is clearly pointed out. "The Network contains more than one current path".There are rules that should be followed for error-free operation. Here compiler is helping and pointing out that error.For complex LAD logics, try using branches. See the following topics: Rules for the use of LAD elements (STEP7 Professional V11) Rules for the use of LAD elements (STEP 7 Basic) Best regards Hamid Hosseini |
Last edited by: hdhosseini at: 11/16/2012 5:07 PM |
|
11/17/2012 7:09 PM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365)
|
Dear vipz, It is not difficult to see "%I0.2" is checked via a normally open Contact(TIA.jpg ). To read more about contacts and coils for STEP7 Basic, please chck it here: Bit logic contacts and coils Best regards, Hamid Hosseini |
11/19/2012 7:45 PM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365) |
is it wrong?? Hello, Writing on inputs (e.g %I0.0) are possible as they are parts of process image (section in system memory) as shown in attachment.I think that is not cause of mentioned error. Please read the following section from online manual of STEP7 in the attachmnet (PII). Best regards Hamid Hosseini AttachmentPII.zip (327 Downloads) |
Last edited by: hdhosseini at: 11/19/2012 7:49 PM |
|
This contribution was helpful to1 thankful Users |
Follow us on