4/27/2020 10:25 AM | |
Posts: 1 Rating:
|
AZRAIQI-V, did you able to connect with two clients to one server on the same port? Or you created 2 servers, one on each port on the same controller and had 2 different clients connected to each of them? Currently, I have 1 controller with 1 server on default port 502 and I'm not able to create two connection in parallel using libmodbus in Cpp I'm trying to create two clients on the same PC to allow multi-threading Only the second client that is connected to server is able to receive information the first client to connect is returning error num=104, "connection reset by peer" Thank you, ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/27/2020 13:36:06New subject after splitting |
|
Follow us on