4/11/2017 3:15 PM | |
Joined: 8/7/2014 Last visit: 2/15/2024 Posts: 13 Rating: (0) |
Hi, can somebody help me to figure out this issue, I am not able to use Technology ojects in S7 1214C wit TIA 13 V SP1. I have connected S110 drive over profinet and getting error of encoder while commissioning, Pl. refer the image below. While adding drive and encoder it is showing error, is there any requirements? to use technology objects.
------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 4/12/2017 2:11:44 PMNew subject after splitting |
|
4/11/2017 3:50 PM | |
Joined: 5/12/2006 Last visit: 4/19/2024 Posts: 22212 Rating: (2979)
|
give details over configuratiopn. which telegram you use and which error is displayed? |
Follow us on