1/25/2011 12:02 PM | |
Posts: 31 Rating: (1) |
Hello to all, very interesting. I've a similar problem. I explain. On the S7-400H manual is reported the scheme for the redundant peripheral with 2 IM153-2, and eventually, with 2 PS. On the hardware configurationis not possible to insert 2 IM153 on the same bus. My question is:the schemeshows 2 IM153-2 to rapresent a single card with 2 Profibus ports or 2 IM153-2 with 1 Profibus port? Attached the image reported on manual. Thanks Splitted from CPU 414 & ET200M. |
Last edited by: O_Moderator at: 1/25/2011 12:12 PMnew subject after splitting |
|
1/25/2011 1:05 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello, 6ES7153-2AR03-0XA0 means SIMATIC DP, ET200M-RED.-BUNDLE CONSISTING OF TWO IM153-2HF (-2BA02) AND ONE BUSMODULE IM/IM 6ES7195-7HD10-0XA0. Hardware configuration will looks different then manual, (then reality). Will looks like Ammy's attached file.( H System.pdf ) but only two IM153-2 connected modules. Best regards, Hristo Mihalev |
12/15/2014 4:54 PM | |
Joined: 11/24/2014 Last visit: 5/8/2024 Posts: 4 Rating: (0) |
thanks for all. |
5/4/2018 7:30 AM | |
Joined: 6/19/2017 Last visit: 5/8/2024 Posts: 8016 Rating: (163) |
New question published by jefesson is split to a separate thread with the subject SM321 compatibility. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on