3/14/2015 5:13 PM | |
Joined: 12/18/2014 Last visit: 9/20/2024 Posts: 33807 Rating: (4200) |
Which logo it should be? 0BA5 or 0BA6 or ...? |
3/14/2015 5:59 PM | |
Joined: 12/18/2014 Last visit: 9/20/2024 Posts: 33807 Rating: (4200) |
Here is a possible solution, works from 0BA5. The program comes in the next post. |
3/14/2015 6:00 PM | |
Joined: 12/18/2014 Last visit: 9/20/2024 Posts: 33807 Rating: (4200) |
Here is the program.
Attachmentfloor_lighting_(0BA5).zip (170 Downloads) |
3/15/2015 10:34 AM | |
Joined: 12/18/2014 Last visit: 9/20/2024 Posts: 33807 Rating: (4200) |
Perhaps this possible solution is the right one. |
Last edited by: ixo65 at: 3/15/2015 3:44:15 PM |
|
3/15/2015 10:35 AM | |
Joined: 12/18/2014 Last visit: 9/20/2024 Posts: 33807 Rating: (4200) |
Here's the program.
Attachmentfloor_lighting_(0BA5)_V2.zip (165 Downloads) |
Last edited by: ixo65 at: 3/15/2015 3:44:41 PM |
|
This contribution was helpful to1 thankful Users |
3/15/2015 4:30 PM | |
Posts: 13 Rating: (0) |
Hi in regards of the post of ixo65 I use a 0BA6 Logo. The Second program works like a charm Many thakns |
This contribution was helpful to1 thankful Users |
Follow us on