12/16/2009 9:06 AM | |
Joined: 4/24/2006 Last visit: 3/28/2024 Posts: 8610 Rating: (1144)
|
Dear Dalie, Are you already using Hotfix 2 for WinCC flexible 2008 + sp1? You can download hotfix 2 from this link: hotfix for WinCC flexible 2008 + Servicepack 1 Or try to perform an OS update with the option 'Reset to factory settings' Have a look at this link: how do you do an operating system update (OS update) on operator panels? Best regards, Wizard |
12/17/2009 9:27 PM | |
Joined: 9/28/2005 Last visit: 3/12/2024 Posts: 2957 Rating: (242)
|
Why ? What error message do you get ? |
Best regards, |
|
12/21/2009 2:36 PM | |
Posts: 4 Rating: (0) |
Hello, The OS-update is not working to solve the problem. The update it selve was working 100%. Best regards, Dave |
Follow us on