9/16/2014 11:26 AM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating:
|
Hello KRS2008104567, 1. Protool for OP7 -Wincc Flexible max. 2008 SP2 for OP77B with SP3 you can't migrate a Protool project and WinCC Comfort (TIA Portal) or higher for KP400. MIGRATION FROM PROTOOL to WINCC FLEXIBLE 2008 SP3 2. What transfer options are available in the various operator panels ... 3. Migration from OP7 to OP 77B http://support.automation.siemens.com/WW/view/en/18796902 Migration from OP77B to KP400 Migration WIncc Flexi to TIA V11 and HMI-Migration - Migration made easy4. No need maintenance for panelManual wrote: The HMI device is designed for maintenance-free operation. However, you should clean the keyboard membrane and the display unit at regular intervals. 5. They are Siemens 6. This forum 7. For the prices you hear the Siemens office near you |
Last edited by: Ste39 at: 9/16/2014 11:30 AM |
|
This contribution was helpful to
1 thankful Users |
9/25/2014 12:40 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating:
|
Best regards Min_Moderator |
Follow us on