Industry Online Support
Technical Forum
5/15/2008 9:37 AM | |
Joined: 4/29/2007 Last visit: 3/15/2021 Posts: 26 Rating: (1) |
Hello, I've found the best way to raise Operator Messages from SFC is as shown here: http://support.automation.siemens.com/WW/view/en/22971603"How do you configure an Operator Request in an SFC Type?" It works well and I'm happy But... I'd now like to embed the current notetext as defined in the SFC Type's Characteristics and determined by the current value of OPTIPNO in the message text being raised. I'm thinking along the lines of settingAUX_PR0X to point to the location of the current NoteText string location. Is this possible? Or are the NoteTexts sent tothe WinCC project upon compilation (much like enumerations). I'd really like my messages to say the same thing as the NoteTexts shown on the faceplate and not just "Operator prompt" Many thanks. John |
Follow us on