(9)| 4/20/2017 2:32 PM | |
|
Joined: 4/28/2015 Last visit: 4/24/2025 Posts: 3345 Rating:
|
Here is an list of tested WIFI devices. WIFI USB Sticks (Plug&Play / no additional drivers needed):
----------------------------------------------------------------------- mPCIe WIFI cards (additional driver needed): drivers available here. You have to copy the driver file "iwlwifi-6000g2b-6.ucode" to /lib/firmware Please feel free to add other working devices which you have tested! Best regards! |
Last edited by: bergmanu at: 8/8/2017 1:22:19 PMLast edited by: bergmanu at: 01/08/2021 12:31:19Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to
|
|
| 5/27/2017 10:56 AM | |
|
Posts: 25 Rating:
|
Hii Bergmanu, can you please explain the step by step procedure to access wifi using intel centrino advanced -n 6235 card. I have copied the driver file to location mentioned. thanks in advance |
| 6/3/2017 7:51 AM | |
|
Posts: 25 Rating:
|
Hii, Thanks for your valuable support. Now wifi is working fine. |
This contribution was helpful to
|
|
| 12/12/2017 9:32 AM | |
|
Joined: 4/28/2015 Last visit: 3/12/2025 Posts: 578 Rating:
|
Exactly this has happened in master of https://github.com/siemens/meta-iot2000. If you are able to build your own image, please give it a try and provide feedback. We are going to release that version officially as well, but that's currently delayed due to non-technical issues. |
This contribution was helpful to
|
|
| 3/9/2018 10:39 AM | |
|
Posts: 8 Rating:
|
Does Atheros AR5BXB63 work ? |
| 3/20/2018 6:21 PM | |
|
Posts: 4 Rating:
|
In the past few days i'm trying to use the following miniPCIe board but without success. https://techship.com/products/option-gtm671wfs/# The module powers up and responds to AT commands but the sim card is not recognized. Anyone know where the miniPCIe header in the IOT2040 is connected to? More precisely the pins 16 UIM_VPP,14 UIM_RESET, 12 UIM_CLK, 10 UIM_DATA and 8 UIM_PWR as explaned in https://support.industry.siemens.com/cs/ww/en/view/109741658 section 7.5.3.3 Mini PCIe interface. Thank you, Nuno |
Last edited by: nuno407 at: 3/20/2018 6:51:34 PMLast edited by: Jen_Moderator at: 3/23/2018 7:51:09 AMOptimized link. |
|
| 3/22/2018 11:13 AM | |
|
Joined: 4/28/2015 Last visit: 4/24/2025 Posts: 3345 Rating:
|
Hi, it looks like the UIM interface can't be used on the IOT, because it is not supported on the hardware. You have to use either a "mPCIe module with integrated SIM Card" or a "mPCIe module with SIM Card Connector". For this there are some Telit cards. Best regards! |
|
Not working for IOT2050 support anymore from March 1st, 2024. |
|
| 7/4/2018 4:20 PM | |
|
Joined: 4/28/2015 Last visit: 4/24/2025 Posts: 3345 Rating:
|
Hi, there is a description how to use the Telit HE-910 D on github. Looks like he made his own image, but there is also a link in the history where you can find the kernel modules to activate. Best regards! |
|
Not working for IOT2050 support anymore from March 1st, 2024. |
|
| 10/25/2018 3:35 PM | |
|
Posts: 7 Rating:
|
Ralink RT5572 based Wifi USB Adapter works fine! Product example: CSL 300Mbit USB WLAN |
This contribution was helpful to
|
|
| 12/17/2018 11:57 AM | |
|
Joined: 4/28/2015 Last visit: 4/3/2025 Posts: 8 Rating:
|
Hello, does anyone know a WLAN stick the Plap & Play works with 5GHZ? |
| 12/17/2018 11:58 AM | |
|
Joined: 4/28/2015 Last visit: 4/3/2025 Posts: 8 Rating:
|
Plug&Play / no additional drivers needed ? |
| 12/17/2018 11:59 AM | |
|
Joined: 4/28/2015 Last visit: 4/3/2025 Posts: 8 Rating:
|
Plag and play or install the Driver? |
| 8/6/2019 2:42 PM | |
|
Posts: 7 Rating:
|
I figured out how enable 3G/4G connection using Huawei E3531 stick. You can add it to the tested dispositives! |
| 5/22/2020 5:32 AM | |
|
Joined: 4/28/2015 Last visit: 10/3/2025 Posts: 40 Rating:
|
Telit HE910 3G Radio Works Telit LE910-NA1 4G Radio Works |
| 8/4/2020 9:47 PM | |
|
Posts: 1 Rating:
|
Qualcomm Atheros AR9462 Wireless Network Adapter installed in iot2040 and is working plug and play |
This contribution was helpful to
|
|
| 9/11/2020 11:03 AM | |
|
Joined: 4/20/2016 Last visit: 2/11/2024 Posts: 1 Rating:
|
Hi, has anyone tried Huawei E3372, LTE USB Stick? |
Last edited by: djgaby at: 09/11/2020 11:04:16 |
|
| 8/18/2021 12:56 PM | |
|
Posts: 1 Rating:
|
Is Edimax Ew-7612UAn V2 working? |
| 6/19/2023 7:21 AM | |
|
Posts: 8171 Rating:
|
New question published by AndrewZaw is split to a separate thread with the subject Need a step-by-step guide for wireless access with Intel Centrino Advanced -N 6235 card. Best regards |
| 10/18/2024 9:47 AM | |
|
Joined: 9/12/2024 Last visit: 11/7/2025 Posts: 3 Rating:
|
I could not get any of the wifi devices on your list so i took a chance and ordered a USB WIFI Adapter for Raspberry Pi from The Pi Hut SKU: 100010
USB WiFi Adapter for Raspberry Pi | The Pi Hut and it works fine, thanks for your help and hopefully this will be of use to other people |
| 11/12/2024 7:46 AM | |
|
Joined: 9/9/2024 Last visit: 5/17/2025 Posts: 1 Rating:
|
TOTOLINK N150USM works plug and play. |
Follow us on