4/27/2017 11:39 AM | |
Joined: 7/30/2012 Last visit: 9/16/2024 Posts: 335 Rating: (12) |
Hi... I'm having Problem In Execution Of External Encoder Homing I'm Using D-425 DP/PN And 6FX2001-5FD13-1AA0 As a External Encoder (Drive Cliq) I Have Configured External Encoder In SCOUT Program (IPO) Other Than Homing Its Working Fine (Updation of position ) I have attached Screenshots Of Program Can Anyone tell me What is the Procedure Of External Encoder Home Function ? AttachmentMCC.zip (343 Downloads) |
4/27/2017 1:44 PM | |
Joined: 7/30/2012 Last visit: 9/16/2024 Posts: 335 Rating: (12) |
Hi... Thanks For Your Reply Encoder Homing Function Only Not Working Yes I'm Starting Task For Encoder Homing From Program I Have Not Received Any Return Value From Encoder Home Instruction (Its Showing 0 Only) Kindly Refer Attachments AttachmentReturn Value.zip (336 Downloads) |
4/30/2017 7:18 PM | |
Joined: 7/30/2012 Last visit: 9/16/2024 Posts: 335 Rating: (12) |
Hi... can anyone tell me what's wrong with my logic or settings? |
5/8/2017 7:41 AM | |
Joined: 7/30/2012 Last visit: 9/16/2024 Posts: 335 Rating: (12) |
Hi Thanks For Reply Will Check and Revert Back |
Follow us on