5/12/2017 7:20 AM | |
Joined: 3/14/2008 Last visit: 10/8/2025 Posts: 2218 Rating:
|
Hi Normally, these alarms can popup when an alarm message block or a technological block (like valve/motor etc) is removed from CFC charts while WinCC is in runtime. I've had several problems with this as well, but I solved them every time by restarting WinCC runtime on the server(s). Possibly you have to do it twice-> Exit runtime, Start runtime, Exit runtime, Start runtime. Maybe the following FAQ's can help you... Did you change anything in the multiproject and downloaded to the PLC? Or does this suddenly occur? If it suddenly happens--> then a wild guess--> Do you have blocks which can generate messages and you are using input "EN" to disable the function of the block? |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on