8/21/2020 8:24 AM | |
Joined: 5/6/2020 Last visit: 9/3/2020 Posts: 6 Rating:
|
Hello, I have an inject node in my flow in which I add a JSON object to the payload. This is followed by a JSON object that converts my object from the inject node. Now there is a function node that assembles my file name in msg.filename and I would like to pass on the value that is in msg.filename as a path to the SMB node. If I enter the parameter msg.filename in the path of the SMB node, I get the following error message: STATUS_OBJECT_NAME_NOT_FOUND (0xC0000034): The object name is not found. "If I write the file name hard, the whole thing works. How can I use the variable msg.filename in the Specify the parameter path in the SMB node or do I have to do this with other nodes? I have included my flow as an attachment so that you can import it if necessary. best regards AttachmentFlows.zip (9 Downloads) |
8/24/2020 7:45 AM | |
Joined: 5/6/2020 Last visit: 9/3/2020 Posts: 6 Rating:
|
Hello everybody, best regards AttachmentFlows.zip (9 Downloads) |
Follow us on