Industry Online Support
Technical Forum
10/14/2008 2:18 PM | |
Posts: 487 Rating: (44) |
Well, You know the problem . Jokes apart,once you have an incompatible OS, it is very difficult to predict the problems and what causaed it. Moreover evenif you call tech support, the first thing they will ask you is to change OS or update your WinCC. There is also incomtibilty with simatic net. 2005 HF1 is only supported by WinCC 6.0 SP4. I would suggest you to correct the compatibility issues. Check the FAQ below for compatibility matrix. http://support.automation.siemens.com/WW/view/en/21927773 |
10/15/2008 5:21 PM | |
Posts: 134 Rating: (11) |
solved it. Solution is Wincc 6.0 SP3 Hotfix2,and reseting Archives I really hope that incompatibillity wil not cause more errors...
|
10/15/2008 6:34 PM | |
Posts: 1275 Rating: (123)
|
Hi Janac, Compatibility can cause unexpected errors in the future... so.. maybe you should think about getting an upgrade for WinCC... You can see the compatibility list here. WinCC v6.0 SP4 is compatible with Windows 2003 SP1 Server Standard. The upgrade from v6.0 SP3 to v6.0 SP4 is free, and you can get it through this link. However, notice you'd have to use the Windows 2003 SP1 Server... WinCC v6.2 SP2 is compatible with Windows Server 2003 R2 SP2, but the upgrade license from v6.0 to v6.2 is charged. You can get some further info on the upgrade license on this link. Before changing any version for any Siemens software be sure to perform a full compatibility check! Best regards, Danielle |
Last edited by: Danielle at: 10/15/2008 6:37 PM |
|
Follow us on