Industry Online Support
Technical Forum
12/4/2013 2:45 PM | |
Joined: 12/4/2013 Last visit: 10/3/2023 Posts: 4 Rating: (0) |
I want to Design a fully Drawout feeder with SIMOCODE PRO V but for a profibus communication I unable to to design a system, Is there any provision ? Panel Make is ELSTEEL. I have Created one option for that a pdf is attached with
AttachmentSimocode Feeder.pdf (177 Downloads) |
12/9/2013 10:27 AM | |
Joined: 5/17/2010 Last visit: 5/22/2024 Posts: 226 Rating: (28) |
Hello, if I understand right you are looping the PROFIBUS line through your drawable unit. This means your PROFIBUS line is interrupted when the unit is drawn out and all other devices behind this unit are not longer available. It is very common to connect withdrable units by passive spur lines to the PROFIBUS but this also brings somerestrictions like max. transmission rate, cable length. (PROFIBUS official does not allow star topology but spur lines behave like a star). Please find further details on spur lines at the SIMATIC NET PROFIBUS Network Manual http://support.automation.siemens.com/WW/view/en/35222591 Best Regards |
------------------------------------------------------------------------------------------------ |
|
Follow us on