(1)| 6/19/2009 4:47 PM | |
|
Posts: 116 Rating:
|
Hi, Can you tell me at what baud you are communicating between DP master and slave? Regards Paresh |
| 6/19/2009 10:39 PM | |
|
Posts: 45 Rating:
|
Hi |
Last edited by: gumis at: 6/19/2009 10:40 PM |
|
| 6/20/2009 2:24 AM | |
|
Posts: 139 Rating:
|
The image of the data you posted looks like a token exchange message. |
This contribution was helpful to
|
|
| 6/20/2009 11:24 AM | |
|
Posts: 116 Rating:
|
No, Master passes token to itself if there is no any other master present within network. Master never passes token to slave. Please find the attached image of Profitrace software in which I have highlated such frame. As far as 9.6 Kbps speed is concerned, I still doubt whether you will be able to see exact frames or bytes Thanks and Regards Paresh AttachmentProfitrace.zip (502 Downloads) |
| 6/20/2009 2:22 PM | |
|
Joined: 10/7/2005 Last visit: 12/29/2025 Posts: 3052 Rating:
|
Hey guys 9.6 Kbps is a supported Profibus DP baudrate. The only difference thatgumis would see at this speed though is a change in the time base of his oscilloscope recording (apart from possibly aslightly "cleaner"square waveform). For your info gumis you will "see" at least 4 messages in your setup per bus cycle which are (am I correct in assuming that this still comprises of one PLC and one PPO3 drive and nothing else?): 1.) SD2 (request) message from PLC to drive (outputs to drive, this will be 13 Bytes long all up with 2 Words of net data for PPO3). 2.) SD2 (response) message from drive toPLC (inputsto PLC, this will also be 13 Bytes long all up with 2 Words of net data for PPO3). 3.) SD1 message (aka FDL status request, PLC "pings" for another master, 6 Bytes long). 4.) SD4 message (token passing, in this case PLC passes token back to itself, 3 Bytes long) For completeness, every so often (e.g is SYNC or FREEZE commands are used or Master enters CLEAR state or periodically at a rate of 3*WDT) you'll also "see" aso called Global control message on the bus (coincidentally also 13 Bytes long and of SD2 type) Nothing else to add since Anchobi said it all and good on him for recognising the captured (Oscilloscope) message as a token passing one (I concur with his assertion as it is too short to be anything else). Cheers Fritz |
Last edited by: fritz at: 6/20/2009 3:43 PMCheers |
|
This contribution was helpful to
|
|
Follow us on