9/15/2014 11:50 AM | |
Posts: 162 Rating: (8) |
OK Thanks. That means there's no new functionnalities for S7-300/400 for Profibus/Profinet Diagnosis ?
|
9/15/2014 11:59 AM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2985) |
Hello, yes this is correct, no new functionality. Regards Christoph |
4/15/2016 10:17 AM | |
Joined: 5/28/2008 Last visit: 5/15/2024 Posts: 1343 Rating: (141)
|
For S7-300/400 are no new functionalities available in TIA. TIA is just the engineering platform. Functionality is done in Firmware, and they had not changed. Softwareblock FB126 is not compatible in TIA environment. For Diagnostic in S7-1200/1500 a lot of new functions are available and also the integrated system diagnostic is much better. Here a really good application example https://support.industry.siemens.com/cs/ww/en/view/98210758 Furthermore, I found some links for S7-300/400 https://support.industry.siemens.com/cs/ww/en/view/101906697 https://support.industry.siemens.com/cs/ww/en/view/2190197 |
This contribution was helpful to1 thankful Users |
Follow us on