4/15/2019 3:19 PM | |
Joined: 12/7/2016 Last visit: 4/5/2024 Posts: 1 Rating: (0) |
Thanks for the link, this link is very very useful and I am able to complete this without and error or issue. But at the end, All addresses in tag table are "false" or "16#0000" when monitoring. Could you please help what are the rest? How to read these addresses? Either these needs to configure in cognex camera? If YES then How? Or still something could be missing in Siemens program? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 4/16/2019 10:36:40 AMNew subject after splitting |
|
4/16/2019 12:45 PM | |
Posts: 1368 Rating: (126) |
Hello WaqasAkram, I do not know the camera so I only have a guess. Do you activated "PROFINET" as protocol in the settings of camera? Sometimes, this is not enabled as default. Perhaps this could help as well http://www.cognex.com/support/downloads/ns/4/20/58/CommunicationsAndProgramming4.0.pdf Page 42ff. |
Follow us on