Industry Online Support
Technical Forum
12/6/2009 9:49 AM | |
Joined: 5/28/2008 Last visit: 4/15/2024 Posts: 4505 Rating: (835) |
Dear Sonnich Jensen, Please find here under the error description & remedy; Error No: 257:90 Error Text:The project '%1' contains errors in the internal data structure. Error Cause: Project data damage by a crash/power failure on the computer. With the "Details" button you can receive more information on the error, if available. Remedy: 1. Close all the STEP 7 applications except the SIMATIC Manager. 2. With the menu command "File > Save as (with reorganization (slow)) " create a of the project which you can then continue to work with. Because of the faults in the existing project, this copy might not contain all the data of the original project. Regards, |
Ayman Elotaify |
|
This contribution was helpful to4 thankful Users |
12/7/2009 8:20 AM | |
Posts: 378 Rating: (47) |
Maybe these two threads can also help you " the project SPPA_T3K contains errors in the internal data structure". Error (257:90). best regards bilao |
This contribution was helpful to1 thankful Users |
Follow us on