4/5/2010 6:18 PM | |
Joined: 4/19/2008 Last visit: 2/9/2024 Posts: 1525 Rating: (159) |
Hi Dikov, You Can Used the Simatic Logon, In that no one Can open the PLC Program Without The Windows Login, or if Some Try to open It Required the Simatic Login Password. Please have a look (Access Protection for Projects and Libraries) |
Ammy |
|
4/6/2010 7:45 AM | |
Posts: 2348 Rating: (263) |
You can assigh IP address protection in HW-Konfig, so PLC would be accessible only from list of addresses. |
4/7/2010 9:06 AM | |
Posts: 2348 Rating: (263) |
HW Konfig->CP(not Lean, Standart or Advanced)->properties ->IP Access Protection :^) |
Last edited by: Aret at: 4/7/2010 9:07 AM |
|
4/8/2010 8:22 AM | |
Posts: 2348 Rating: (263) |
Yep, unfortunately it's so. Generally protection can be done by means of router/switch by creating VLAN:^) |
This contribution was helpful to2 thankful Users |
4/9/2010 10:37 AM | |
Joined: 4/2/2010 Last visit: 4/22/2024 Posts: 3 Rating: (0) |
Thanks friends. Probably I will use IP protection + router :) |
Follow us on