7/16/2019 10:59 PM | |
Joined: 4/28/2015 Last visit: 8/9/2019 Posts: 10 Rating: (0) |
Hi Fe_lipe, Do you have any experience with available python or C/C++ implementations for IOT2000 which you could share with us? I found the following: Python: FreeOpcUa ? C/C++: tbd. Points your instability concern only to OPC UA server implementation based on Node-RED or do you also have issues with OPC UA Client based on Node-RED? Thank you in advance. Lars |
Last edited by: Jen_Moderator at: 07/17/2019 14:03:07Optimized headline. |
|
7/17/2019 2:12 PM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating: (60)
|
Hello, The python examples are platform independant, so you can use them as is after you install the freeopcua package:
As for C/C++, I would suggest using open62541 and programming the server in Eclipse. We have an open62541 Client example coming soon, but no server example planned. OPC UA Clients run stable in node-red. It's just the Server node which causes node-red to crash after about an hour. Kind regards! |
This contribution was helpful to1 thankful Users |
7/17/2019 9:11 PM | |
Joined: 4/28/2015 Last visit: 8/9/2019 Posts: 10 Rating: (0) |
Thank you Fe_lipe for answering so fast |
Follow us on