5/13/2021 8:14 PM | |
Joined: 4/9/2021 Last visit: 8/25/2023 Posts: 1 Rating: (0) |
I have to replace MP 377 12" with TP 1200 Confort, does siemens make any retrofit kit for TP1200, because MP 377 12" is bigger. thanks ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 05/14/2021 14:59:35New subject after splitting |
|
5/17/2021 7:03 PM | |
Joined: 4/25/2016 Last visit: 3/31/2023 Posts: 115 Rating: (13) |
Hi! I'm not sure about what you refer with a retrofit kit. The steps for a migration of a MP 377 12" to a TP1200 Comfort are: 1- Migrate to WinCC Flexible 2008 SP3/SP5. 2-Migrate to TIA. If project its in WinCC Flexible 2008 SP3 you can migrate to V13 SP1/SP2 or V14 SP1. If project its in WinCC Flexible 2008 SP5 you must migrate to V14 SP1 Upd 2 (or a newer update). You can't migrate directly to a newer TIA version because WinCC Flexible panels are not supported in TIA since V15 3- Change the panel to TP1200 Comfort. 4- Open project with V15/V16. Maybe this manuals or FAQs will help you: SIMATIC HMI WinCC flexible 2008 8 Migration https://support.industry.siemens.com/cs/ww/en/view/18796902 Migration of a WinCC flexible project integrated in STEP 7 V5.x to WinCC (TIA Portal) and upgrading of the operator panel version after a change of the WinCC (TIA Portal) version to a newer version. https://support.industry.siemens.com/cs/ww/en/view/77430539 Migration Tool TIA Portal https://support.industry.siemens.com/cs/ww/en/view/58638200 If you don't have the original project of the panel there is a service of migration from a bakcup: https://support.industry.siemens.com/cs/ww/en/view/109765132 If you need a more specific service you should contact you local Siemens contact. Best regards. |
Follow us on