4/26/2013 1:31 PM | |
Joined: 3/14/2008 Last visit: 4/13/2024 Posts: 2064 Rating: (926) |
Hello, |
Last edited by: Oreca at: 6/5/2013 11:08 AMEdit: changed post Last edited by: Oreca at: 4/26/2013 2:36 PMIf I could help you, you can use the RATE button. Thank you. |
|
4/26/2013 5:58 PM | |
Posts: 836 Rating: (99)
|
Thanks for sharing |
6/5/2013 11:10 AM | |
Joined: 3/14/2008 Last visit: 4/13/2024 Posts: 2064 Rating: (926) |
Updated post, problem definition |
If I could help you, you can use the RATE button. Thank you. |
|
6/10/2013 4:05 PM | |
Joined: 3/14/2008 Last visit: 4/13/2024 Posts: 2064 Rating: (926) |
Well, cant do anything in the compatibility list, can't select an ipc and pcs7 software. Anyway the SR is 1-3090557078. Siemens didn't say it isn't compatible, and now three weeks have past... SP1: Simatic NET 2005, v6.3+HF1 SP4: Simatic NET 2005, v6.3+HF1+HF11+HF15+HF18+HF19 |
If I could help you, you can use the RATE button. Thank you. |
|
6/10/2013 4:26 PM | |
Joined: 3/14/2008 Last visit: 4/13/2024 Posts: 2064 Rating: (926) |
Well, Tried installing Windows Server 2003 SP1, I saw in the firmware list of the CP1613, in Simatic NET that Windows Server 2003 SP1 is supported as of 6.31. But when trying to install 2003 SP1 on the IPC847C I constantly get an error... also with Windows Server 2003--->BSOD screen...so not working on ipc847c Seems it's a deadlock situation... |
Last edited by: Oreca at: 6/10/2013 4:28 PMIf I could help you, you can use the RATE button. Thank you. |
|
6/10/2013 4:34 PM | |
Posts: 836 Rating: (99)
|
Did you try to reinstall the CP1613 like proposed by support? |
6/11/2013 8:19 AM | |
Joined: 3/14/2008 Last visit: 4/13/2024 Posts: 2064 Rating: (926) |
Yes, I did, Uninstalled all WDM1613 reg files as proposed. I also set up the pc without installing hardware automatically and installed the driver manually. Also I rerun Simatic NET installer from the toolset cd like proposed. I also checked the register values from the SP1 and SP4, A few were different, but changing them to the SP1 values, didn't help either. There was one string value in regedit: IsDeact = YES. I changed that one to NO and then the card wasn''t deactivated anymore. But restarting the PC sets the default value back somehow. |
If I could help you, you can use the RATE button. Thank you. |
|
6/11/2013 9:18 AM | |
Joined: 3/14/2008 Last visit: 4/13/2024 Posts: 2064 Rating: (926) |
Yeah, But then in Set PG/PC interface, the card has still an exclimation mark above it that states: module faulty or deactivated.. But maybe i can write a batch file and test it if it actually works... |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on