7/30/2010 3:58 AM | |
Posts: 691 Rating: (36) |
I have tried all these things |
5/2/2015 12:25 PM | |
Joined: 2/29/2012 Last visit: 5/4/2024 Posts: 17 Rating: (3) |
Hello, Stop Sql server Delete Wincc building files |
5/28/2017 2:52 PM | |
Joined: 12/9/2010 Last visit: 10/8/2022 Posts: 623 Rating: (76) |
Hi Niranjan Prasad, U should try <SHIFT> + <ALT> or <SHIFT> + <CTRL> combination. Open projectWhen you start WinCC the first time, the WinCC Explorer is opened without a project. Whenever you start WinCC again, the last project you had open will be opened again. With the key combination <SHIFT> + <ALT>, you can prevent WinCC from opening a project immediately. Press the <SHIFT> key and the <ALT> key while WinCC is opening. Keep the keys pressed until the window of the WinCC Explorer is displayed. The WinCC Explorer opens without opening a project. Activated ProjectIf the project was activated when you exited WinCC Runtime, it will be opened in Runtime again when you restart WinCC. If you close a project and open another project that was opened the last time in the activated state, WinCC once again opens the project in Runtime. With the key combination <SHIFT> + <CTRL>, you can prevent WinCC activating Runtime immediately. Press the <SHIFT> key and the <CTRL> key while WinCC is opening. Keep the keys pressed until the project is open and displayed fully in the WinCC Explorer. WinCC opens the last project without starting Runtime |
If you like the comment, rate it (right top) or thank it (left bottom). |
|
This contribution was helpful to2 thankful Users |
Follow us on