Industry Online Support
Technical Forum
6/24/2009 9:19 PM | |
Posts: 133 Rating: (13) |
Hello, Has anyone set up Easy Positioning module with just the BOP or Script file. I am looking for how to enable the EPOS module without STARTER. |
6/24/2009 11:09 PM | |
Posts: 2 Rating: (1) |
Drives_Coach, This can be done; however, setting up the basic positioner with just the BOP is prettytime intensive... I have attached a file that shows the parameters that need to be set to parameterized a S120 single-axis AC drive (with a Drive-CLiQ equipped motor)for servo mode with closed-loop speed control, basic positioner, and extended speed setpoints. Hope this helps. AttachmentParameter List_ServoBasic.pdf (561 Downloads) |
Follow us on