Industry Online Support
Technical Forum
3/4/2011 2:30 PM | |
Posts: 9 Rating: (0) |
I used no. 2. But I am not sure which power factor to set in the motor data in drive? I guess motor power factor changes also? |
3/4/2011 3:12 PM | |
Posts: 344 Rating: (50) |
Power factor will not be affected. The only limitation is that the drive will not be able to achieve rated speed as described in 2 above. |
3/4/2011 3:34 PM | |
Posts: 9 Rating: (0) |
Thanks for replies. I will type in then the same power factor. |
Follow us on