Industry Online Support
Technical Forum
5/2/2011 7:10 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181)
|
Hello Rey, Connecting cable from PG 7xx to programmable controllers AG 90 U ... AG 155 U Best regards, Hristo MIhalev |
5/3/2011 3:07 PM | |
Posts: 376 Rating: (57) |
Hello Rey, here more informationen about the topic S5 connection cable between PC/PG with serial RS232 interface. If you use a PC with serial interface youcan take the PC converter cable with the order number 6ES5734-1BD20. The interface assignment of the PC converter cable finds you here: http://support.automation.siemens.com/WW/view/en/13063839 Here a further recommendation. Köster-Box (PC-S5-Interface) Interface for programming Siemens S5-PLCs with the PC. The Kösterbox converts the RS232 signals of the PC into TTY signals (20mA) of the automation system. • The box is full duplex, send- and recieve channel, • the box is active for programming S5 90-115U, • for S5-135/155U and CP or acting passively with other cable, • the box has its own power supply with galvanic separation Her the link: http://www.koester-systemtechnik.de/Koester_Box_E.html If you usea Field PG, Power PG or PG7xx to connect theS5-ControllersAG 90U to AG 155U, you can use the cable with the order number 6ES5734-2BD20. More information about the cable finds you here: http://support.automation.siemens.com/WW/view/en/217863 I hope this information helps you. Best Reagards Gucci |
Follow us on