2/26/2019 1:58 PM | |
Joined: 7/3/2018 Last visit: 5/28/2024 Posts: 3 Rating: (0) |
Thanks for quick answer so I shouldn't do anything in S7 and I don't need them anymore in S7 |
2/27/2019 3:09 PM | |
Joined: 7/3/2018 Last visit: 5/28/2024 Posts: 3 Rating: (0) |
Thanks for your helpful answer, The old S5 135U was connected with other S5 over TCP\IP (VIPA CP143 H1 -TCP/IP), now I want to replace the old CPU andVIPA CP143 H1 -TCP/IP withABC X-CPU-6 m57 and convert the S5-Program to S7-Program and I want to keep the connection over TCP\IP with the other PLC’s. Here are the content of blocks from FB121 to FB127. Attachmentjpg2pdf.pdf (363 Downloads) |
Follow us on