6/25/2019 10:38 PM | |
Posts: 3 Rating: (0) |
hello all, I am new to motion control and I am trying to control a stepper motor. I created an axis based on my requirement. But after that, I cannot do commissioning and the diagnostics show axis error and configuration error. can you guys please check it? I do not know what to do. thank you Attachmentstepper.zip (119 Downloads) |
6/26/2019 9:04 AM | |
Joined: 10/10/2005 Last visit: 4/18/2024 Posts: 1917 Rating: (133) |
Hello s09, in your project there are no the motion control functions, example “MC_Power”. Before a technology object can be enabled without error via "MC_Power", all the necessary sensors (encoders) and actuators (drives) must be available for the technology object. See the FAQ (link) for further informations: Which requirements have to be fulfilled before a technology object can be enabled via "MC_Power"? Cicero |
6/26/2019 3:59 PM | |
Posts: 3 Rating: (0) |
hello thank you for the reply. I did not add MC_power in my program block because the tutorial from Siemens in youtube did not have that, still, it worked perfectly. However, even after adding MC_power in my program block, I have the same configuration error. The error message is "OK", nothing else. What does this mean? I do not think there is an error with the configuration of axis since I just copied the data for the axis that was working in our PLC lab. |
Follow us on