(2)| 9/20/2017 9:22 AM | |
|
Joined: 2/27/2014 Last visit: 8/28/2025 Posts: 689 Rating:
|
Hello Alia, Your right, it should be part of TIA V13 with new update then latest S7 hardware version should be available in V13. But unfortunately this is not possible. With all latest innovation in hardware and software is available in V14. TIA Portal V14 options TIA Portal Multiuser Engineering TIA Portal Multiuser Engineering enables multiple users to simultaneously work on a single project. The basic principle:
TIA Portal Teamcenter Gateway As an integrated option for the TIA Portal, SIMATIC Energy Suite directly links energy management and automation for the first time and thereby creates energy transparency in the production system. In addition, simplified programming of energy-measuring components significantly reduces the configuration work.see also
SIMATIC PLCSIM Advanced SIMATIC PLCSIM Advanced enables you to create virtual controllers for simulating S7-1500 and ET 200SP controllers and provides extensive simulation of functions. Compared to the standard S7-PLCSIM, PLCSIM Advanced offers the following additional functions:
SIMATIC ODK 1500S ODK 1500S enables the development of function libraries with the high-level languages C/C++ for SIMATIC S7-1500 PLCs that support ODK. These function libraries can be loaded and executed directly from the user program. S7-1500 PLCs that support ODK:
SIMATIC Target 1500S™ for Simulink®
SIMATIC Visualization Architect SIMATIC Visualization Architect (SiVArc) enables simple, fast, flexible and automated creation of HMI contents based on the STEP 7 user program.
The following new options are offered exclusively as runtime options for TIA Portal V14. SIMATIC ProDiag Selective and fast machine and plant diagnostics for SIMATIC S7-1500 and SIMATIC HMI:
SIMATIC OPC UA S7-1500 The OPC UA S7-1500 option enables easy connection of any third-party device to the S7-1500 via the OPC UA server integrated in the S7-1500 CPU:
|
|
With Best Regards, |
|
| 9/20/2017 12:49 PM | |
|
Posts: 3 Rating:
|
Thank you very much. |
Follow us on