5/28/2012 7:59 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hello, So, if the battery is healthy it should 'keep' the data for few days (100hours) for sure. (as 200 days max.). For statistic you can try withTest of the Battery module S7-200. As there ia mentioned too to avoid a data loss after the expiry of buffer time, we recommend the storage of data into internal EEPROM of the CPU - see Entry-ID17471561. Be careful with writing in that memory!
Best regards, Hristo Mihalev
|
5/30/2012 12:18 PM | |
Joined: 9/1/2005 Last visit: 9/18/2024 Posts: 4104 Rating: (195) |
closed cause question posted twice. The second thread with the subject S7-200 parameters - why are the lost?is published within the same conference. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on