10/29/2013 11:12 AM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (715)
|
Hello, If you have password, enter it when asked, then change the settings and download again. If no password. There are 3 options: 1. Ask programmer for password. 2.Password for the access to a password-protected S7-200 does not exist 3.Resetting the S7-200 to the factory default settings (WIPEOUT) Regards, Marcjan |
Last edited by: Marcjan at: 10/29/2013 11:14 AMProblem solved? |
|
This contribution was helpful to1 thankful Users |
10/29/2013 2:37 PM | |
Posts: 12 Rating: (0) |
DearMarcjan, Thank for your Reply! I have password from programmer but he create password level 4. In this level 4, if I download Program, data block & system block then download button will be hidden. I can only download program & data block so I can not remove password of PLC. Maybe I have to use Wipeout to factory reset PLC then I will download original program to PLC. With thanks and Best regards, |
10/29/2013 3:28 PM | |
Posts: 12 Rating: (0) |
Dear Marcjan, Thanks for your strongly supports! Regards, |
This contribution was helpful to1 thankful Users |
3/21/2016 8:33 AM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (820) |
Hello, look at this document, check RS-232 and give question to your Siemens partner if it could be purchased, or other suitable product: http://www.profibus-factory.com/wp-content/uploads/2013/07/s7200cableEnglish.pdf |
Last edited by: Duris_I at: 3/21/2016 10:46:39 AMWith best regards... |
|
Follow us on