10/26/2014 12:04 PM | |
Posts: 50 Rating: (2) |
Hi, I use SCL so the sample programming provided is inSCL. I hope it is useful. Regards |
10/26/2014 1:05 PM | |
Posts: 6 Rating: (0) |
It was helpful, thankyou very much. |
This contribution was helpful to1 thankful Users |
10/26/2014 4:49 PM | |
Posts: 6 Rating: (0) |
Hi there, I have attached the archived program that i have written for our panel. it is a panel for demonstration of how plc works. i have 16 switches and 16 leds. which are the digital side of the plc. then we have the analog side where we have 2 potentiometers that supply 0-10 volts input supply to the plc through a 3 position selector switch. the input is displayed by means of a digital voltmeter. the output of the plc, wired from piq272 and piq274 are connected to a digital voltmeter. we need to demonstrate how the scale function works. any value on the output voltmeter that corresponds to the input will be fine. thanks in advance,
AttachmentSimulatorForTraining.zip (304 Downloads) |
Follow us on