3/19/2014 12:09 PM | |
Posts: 7 Rating: (0) |
So mean that we cant config fault tollerent in TIA..? Its sound bad, |
3/19/2014 12:15 PM | |
Joined: 1/28/2009 Last visit: 4/1/2024 Posts: 6836 Rating: (1359) |
Hello, Yes it is not possible, Check the new features of TIA V13 in the following link and there is no note for supporting H-CPUs there. Personally, I prefer using STETP 7 and I believe that it ismore efficient than current versions of TIA Portal. http://support.automation.siemens.com/WW/view/en/84047138 Best regards, |
Last edited by: hdhosseini at: 3/19/2014 1:20 PM// typo |
|
This contribution was helpful to1 thankful Users |
3/19/2014 12:40 PM | |
Posts: 7 Rating: (0) |
Hello Mr. Hamid Thank you for your feed back...its useful link best and regards Raghava Reddy |
2/15/2017 8:46 AM | |
Posts: 73 Rating: (1) |
Hi there, I have the same question about the presence of this cpu in v.14. Is there any one to help us? |
2/15/2017 8:49 AM | |
Joined: 5/12/2006 Last visit: 4/23/2024 Posts: 22221 Rating: (2979)
|
Hello, no S7-400H not supported in TIA V14! Regards Christoph |
This contribution was helpful to1 thankful Users |
3/1/2018 6:40 PM | |
Joined: 7/8/2012 Last visit: 2/21/2022 Posts: 13 Rating: (0) |
what about v15? |
3/2/2018 7:47 AM | |
Joined: 10/7/2005 Last visit: 4/23/2024 Posts: 3004 Rating: (1046) |
Still no support for S7-400 H in TIA Portal V15. Chances are an S7-1500 H will come out later this year and 400 H's will remain the domain of PCS7/classic Step7 (and yes, I am speculating here) |
Cheers |
|
This contribution was helpful to1 thankful Users |
Follow us on