11/22/2011 4:02 AM | |
Posts: 14 Rating: (0) |
this is 412-3h of second project (see attachment) |
11/22/2011 7:32 AM | |
Posts: 14 Rating: (0) |
It looks same but without second DP i'm still looking for a solution |
11/22/2011 8:04 AM | |
Joined: 10/7/2005 Last visit: 4/24/2024 Posts: 3004 Rating: (1046)
|
Hello noname11 sincethe 6ES7412-3HJ14-0AB0 has only ONE MPI/DP port on board (as far as I know anyhow), the only explanation I can offer is that someone configured for example a 414-4H or 417-4H and then changedits module name to 412-3H. Attached is a "silly" pic of a CPU pretending to be a412-3H with 4 DP ports (configuredis in fact a 417-4Hand tow of the"DP ports" are of course sync modules). The only alternative to the above explanantion is that an "unofficial" (or third party) version of the 412-3H exists (which would then also be required to be available for configuration in the HWcatalogue of whoever configured the original system...). Question is: What CPU order number is shown in the bottom half of your screen and/or in the CPU properties? |
Cheers |
|
Follow us on