6/4/2018 8:01 AM | |
Posts: 15 Rating: (0) |
Hi everyone! I have got a redudant system with S7 414-5h cpu's. On Standby CPU always lights Extf led. Can anyone help what should I do to solve this problem? I'll attach a diagnostic buffer. AttachmentDiagnose2.txt (176 Downloads) |
6/4/2018 8:22 PM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365)
|
Dear user,
Please tell us about all CPU LED status in Master and stand-by CPU.As the starting point, you can try checking the slave number #5 over PROFIBUS subnet connected to the "DP master system ID: 2" that is possibly on CPU on rack#1.If you have a faulty slave module or faulty connector, please rectify it.You can go online on HW Config editor with the hints from section 5.3 of THIS MANUAL for more root cause analysis. I hope it helps, hdhosseini |
Last edited by: hdhosseini at: 6/4/2018 8:26:29 PMLast edited by: Jen_Moderator at: 6/5/2018 8:15:31 AMOptimized link. |
|
6/6/2018 8:45 AM | |
Posts: 15 Rating: (0) |
Thank you for your reply hdhosseini I have checked HW in online and saw that the PS 407 is not available there. A few years ago someone has changed PS |
Follow us on