7/2/2013 12:36 PM | |
Joined: 9/23/2005 Last visit: 4/17/2024 Posts: 4325 Rating: (1423)
|
Hi, Here there is a sample program with S7-1500, ET200SP and PROFIEnergy feature. The function is managed directly in OB1 by block Call. The bit memories " " and " " command the function. This sample program was not 100% tested. There are know that in PLCSim it couldn't be tested 100% too. AttachmentS71500 Profienergy.zip (731 Downloads) |
Last edited by: O_Moderator at: 7/2/2013 3:45 PMDenilson Pegaia |
|
This contribution was helpful to1 thankful Users |
4/7/2014 10:28 PM | |
Joined: 9/23/2005 Last visit: 4/17/2024 Posts: 4325 Rating: (1423)
|
Hi, here there is a tested project. "Start Pause" and "End Pause" PLC variables command the HMI. AttachmentC:\Users\z0008iwv\Documents\Bluetooth Exchange Folder\S71500_Profienergy_V13.zip (717 Downloads) |
Denilson Pegaia |
|
4/7/2017 2:02 PM | |
Joined: 10/27/2010 Last visit: 4/19/2024 Posts: 3 Rating: (0) |
Hi, If you make the same PE_START_END for the ET200SP what would be the ID number? Regards Anders |
5/1/2019 9:01 PM | |
Joined: 5/6/2018 Last visit: 2/2/2024 Posts: 13 Rating: (0) |
Hi, You can see it in the System constants I hope it helps, Best Regards |
10/13/2023 11:26 AM | |
Joined: 9/23/2005 Last visit: 4/17/2024 Posts: 4325 Rating: (1423)
|
Hi, The converted program exceeded the size of 5MB enabled for uploads here. You can update it to V13 SP2 and after that open in TIA >V13. Attachmentprint.pdf (256 Downloads) |
Denilson Pegaia |
|
Follow us on