6/19/2020 10:20 AM | |
Joined: 12/13/2016 Last visit: 12/13/2023 Posts: 12 Rating: (1) |
Sorry I'm not familiar with the forum style.....Actually just create 1 new post And my problem is the unit I received 15 pcs are without OS and I saw in the FORUM said that the shipment with out OS. ….Then I need to install the OS into eMMC for my client, can you suggest me? If my understanding was correct, I should use "Example Image" temporary until the official SIMATIC Industrial OS V2.0 released? Another 50 pcs. are coming, I'm not sure will be without OS. Then I'd saw topic name "How to setup the IOT2050" And I'd download the document " Install Example Image on eMMc" but when click download Micro-SD Card Example Image. It's fail.(please see attached) |
6/19/2020 11:02 AM | |
Joined: 12/13/2016 Last visit: 12/13/2023 Posts: 12 Rating: (1) |
done,.send you Personal Message |
Follow us on