5/6/2014 7:27 AM | |
Joined: 12/12/2011 Last visit: 12/30/2020 Posts: 821 Rating: (40)
|
Hi, your user have to be part of the groups "Administrator" and "SIMATIC Logon", With this user you could configure SIMATIC Logon. Best Regards, Healthcheck |
Grundkurs/Systemkurs WinCC V7: |
|
5/6/2014 8:52 AM | |
Posts: 204 Rating: (29) |
hello, Thanks for the reply,now am able to login in wincc runtime,but without enabling runtime am getting previous error. |
5/12/2014 12:11 PM | |
Joined: 12/12/2011 Last visit: 12/30/2020 Posts: 821 Rating: (40)
|
What do you mean with this? You could login in Wincc runtime? But not enabling the runtime? Please explain what do you mean with "enabling runtime" Best Regards, Healthcheck |
Grundkurs/Systemkurs WinCC V7: |
|
5/23/2014 11:00 AM | |
Joined: 12/12/2011 Last visit: 12/30/2020 Posts: 821 Rating: (40)
|
Hi, om all computer you have to create a windowsuser "e.g. userSL". This user should be part of these windows gruops "Administrator" and "SIMATIC Logon". The you could configute SL on the computer. Start SIMATIC Logon configure. Here you could choose the default user, logout time, logon server........ Now it is possible to logon in WinCC on Client 1 with a user "e.g. operator" which is only configured on your Logon Server (Windows user/ groups" Hope this helps you. Best Regards, Healthcheck |
Grundkurs/Systemkurs WinCC V7: |
|
This contribution was helpful to1 thankful Users |
Follow us on