8/19/2016 11:05 AM | |
Joined: 4/2/2016 Last visit: 7/13/2022 Posts: 413 Rating: (6) |
I have SIMODRIVE 611U V14.1 and all settings I configured through this program (OP display not use); We have Simodrive 611U - three motor control system: 6SN1123-1AB00-OHA1 + 6SN1118-0NK01-0AA1 (master) + Motor1FK7042-5AF71-1TA0 +Motor1FK7042-5AF21-1TA0 6SN1123-1AA00-OHA1 + 6SN1118-1NJ01-0AA1 (slave) + Motor1FK7042-5AF21-1TA0 So in one system we have two motor 1FK7042-5AF71-1TA0 (267V) and one motor 1FK7042-5AF21-1TA0 (147V), I configured the parameters for the 167V motor motor stopped heated/sound but I do not know how dangerous it is for the system in general All parameters/nameplate etc. can be found in the annex. I do not understand why technical support said that I can not use this motor 1FK7042-5AF21-1TA0 (147V) in our system6SN1123-1AB00-OHA1 + 6SN1118-0NK01-0AA1? than it is dangerous? by normal this motor1FK7042-5AF21-1TA0 (147V) created for Sinamics 230V, but why it can not be used for Simodrive 611U (600 V DC). if the power converter is enough for this engine what the problem? but now I have other problems: movement going in jerks (not smooth) (maybe need to reduce the proportional gain on the controller); configure master / slave (as shown in Master-slave.png) I will be glad of any help on these questions!!! AttachmentSimodrive 611U and motor 230V.zip (301 Downloads) |
Last edited by: _oleksandr_ at: 8/19/2016 11:09:44 AMLast edited by: _oleksandr_ at: 8/19/2016 11:43:49 AMLast edited by: _oleksandr_ at: 8/19/2016 4:41:40 PM |
|
8/20/2016 10:14 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
How & where you have connected motor resolver feed back to drive? |
Follow us on