11/17/2021 5:42 AM | |
Posts: 1 Rating: (0) |
I had a problem with Spindal Drive Heat Sink Over Temperature. No specific information was available in this regard, therefor I have to dig out the info by Revers Engineering of the both units. It was a difficult work, but I had no choice. Therefore I did it. Both Heat Sinks ( Infeed Unit & Spindal Drive) have 150 Degree Bimetal Temperature Switch. These Switches pass the +15V Supply to the Infeed unit Alarm Monitoring Module X192 on the Supply Board. Some details of Simodrive Equipment Bus have also be needed to dig out to solve the above fault. I am still working on it. I attach the my effort in the form of PDF. I hope this will be helpfull for any body. Thanks Engineer Nasir Ahmed [snip] AttachmentHURCO SPINDAL DRIVE-.pdf (724 Downloads) |
Last edited by: Jen_Moderator at: 11/17/2021 12:12:53Removed contact data, doesn't comply with forum terms. |
|
11/20/2021 6:40 PM | |
Joined: 10/17/2007 Last visit: 4/22/2024 Posts: 3972 Rating: (340)
|
Hi, Friend, you wrote so long but I did not get your point. only information you showing here--SINUMERIC PCU 50.3-C, 1.5GHz 512MB, WinXP Pro EmbSys--It is 840D HMI --belong to CNC, what actually you need help? here is SIMODRIVE branch . And you name the drive--is it Siemen drive or not, send picture here. If you need equipment bus drawing the link in this topic already help you, I attached it again for your convince AttachmentRIBBON_CABLE_DATA.pdf (793 Downloads) |
If you like my comments please |
|
Follow us on