(0)| 1/20/2016 9:49 AM | |
|
Posts: 153 Rating:
|
and Please explain the Function if drive has 2 CUD installed. My old drive is S00 option and new drive is G00 +G11 My old and New Drive rating is same =>60A |
| 1/20/2016 11:42 AM | |
|
Joined: 8/25/2006 Last visit: 12/30/2025 Posts: 2221 Rating:
|
Hello. Yes, you can use peer-to-peer interface to connect Sinamics DCM and Simoreg DC Master, this is described in the manual, chapter 10.29. In the same manual you can read about second CUD, chapter 10.30. Look also at this manual: SINAMICS DCM DC Converter, Application: SINAMICS DCM as field supply unit |
| 1/22/2016 2:08 AM | |
|
Posts: 153 Rating:
|
Hello KSN, Thank you for reply. Actually I read this manual before going to site. it is written as below: ''The peer-to-peer interface enables BICO interconnections across several SINAMICS DCMs, as well as allowing the peer-to-peer interface to establish signal connections between converters in the SINAMICS DC MASTER range (MLFB = 6RA80...) and converters in other ranges, such as SIMOREG DC-MASTER (MLFB = 6RA70...) and SIMOREG K (MLFB = 6RA24...).'' A "peer-to-peer connection" refers to "a connection between partners with equal status". I have Connected New sinamics DCM(for Field) in place of old DC drive, Armature drive is same 6RA70 (1200A). I have done all setting as per given manual for Field Unit in https://support.industry.siemens.com/cs/document/47362177/sinamics-dcm-dc-converter-application%3A-sinamics-dcm-as-field-supply-unit-compact-user-manual?dti=0&lc=en-WW I am using Armature supply +field supply. When i am giving command to the drive, then armatre drive and DCM drive do not send and recieve the data. what could be the problem. If anybody have any experience with Simoreg DC + Sinamics DCM please share the parameters details. Please find my existing setting for Simoreg and sinamics. Thanks in advance. AttachmentPeer2peer.zip (581 Downloads) |
Last edited by: Soni.... at: 1/22/2016 2:09:28 AM |
|
Follow us on